Use Symbol Factory
Symbol Factory is a third-party graphics library that provides a large number of quality graphic elements for industrial automation, including pumps, pipes, valves, tanks, mixers, motors, ducts, electrical symbols, flow meters, material handling, sensors, PLCs, transmitters, and ISA symbols. These graphics can be used on graphic displays.
To open Symbol Factory, use one of these methods:
- In theExplorerwindow, double-clickSymbol Factory.
- SelectObjects > Symbol Factory.
- Drag
from the toolbox.
Help
from the Symbol Factory Options
menu.Provide Feedback