Add an image from Symbol Factory to a graphic object
Use the
Image Browser
to add an image from Symbol Factory as needed while setting up a graphic object.To add an image from Symbol Factory to a graphic object using the image browser
- In theImage Browser, clickLaunch Library.
- Browse through theCategoriesand select the graphic to be used.
- (optional) Modify the graphic options below the graphic tab.
- ClickCopy as.The Symbol Factory minimizes, returning to theImage Browser.TIP: Copy as SVG is not supported.
- ClickPaste from Library.
- Type a unique name for the image and clickOK.The graphic will now be shown in thePreviewwindow. The graphic has been added to the list in theImage Browser. This also adds the image to theImagesfolder in theExplorerwindow.
- ClickOK.
Provide Feedback