Start FactoryTalk View ME Station on a PanelView Plus 7, PanelView Plus 6, PanelView Plus, or PanelView Plus CE terminal
On a
PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, or PanelView Plus CE
terminal, you can disable the automatic startup of FactoryTalk View ME Station
and start FactoryTalk View ME Station
manually.To start
FactoryTalk View ME Station
on a PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, or PanelView Plus CE
terminal, do one of the following:- On the desktop, double-click the shortcut iconFTView ME Station.
- In the Windows Explorer, double-click MERuntime.exe. Default location for this file is:(PanelView Plus 7andPanelView Plus 6)\Windows(PanelView PlusandPanelView Plus CE)\Storage Card\Rockwell Software\RSViewME
- If WindowsStartmenu is available, from theStartmenu, selectRun. In theOpenbox, type the path to the MERuntime.exe file.
- If WindowsStartmenu is available, from theStartmenu, selectPrograms > Rockwell Software >.FactoryTalk ViewME Station
Provide Feedback