Start FactoryTalk View ME Station on a personal computer
On a personal computer, you can set up
FactoryTalk View ME Station
to start automatically when the computer starts or manually start FactoryTalk View ME Station
.To start
FactoryTalk View ME Station
on a personal computer, do one of the following- From WindowsStartmenu, selectAll apps > Rockwell Software >.FactoryTalk ViewME Station
- On the desktop, double-click the shortcut iconFTView ME Station.
- In the Windows Explorer, right-clickMERuntime.exeand selectRun as administrator. Default location for this file is\Program Files (x86)\Rockwell Software\RSView Enterprise\MERuntime.exe
- From WindowsStartmenu, selectRun. In theOpenbox, type the path to the MERuntime.exe file.
Provide Feedback