Start FactoryTalk View ME Station on a MobileView terminal

On a
MobileView
terminal, you can set up
FactoryTalk View ME Station
to start automatically when the terminal starts or manually start
FactoryTalk View ME Station
.
To start
FactoryTalk View ME Station
on a
MobileView
terminal, do one of the following
  • On the desktop, press the
    FTView ME Station
    icon
  • In
    File Explorer
    , right-click
    MERuntime.exe
    and select
    Run as administrator
    . The default location for the file is
    C:\Program Files (x86)\Rockwell Software\RSView Enterprise\MERuntime.exe
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal