Login and logout

For security to be effective, all users must have an Account ID to log in. Set up the IDs in the
User Accounts
dialog box.
To allow users to log in, create a login button in a graphic display that all users have access to, such as the startup graphic display.
To allow users to log out, create a logout button in a graphic display that all users have access to, such as the startup graphic display. When a user logs out, the user becomes a default user. Be sure that the default user privileges are carefully controlled.
You can also set up your runtime terminal to log out the current user automatically after the terminal has been inactive for a specified period of time. The automatic logout is independent of the security configuration of
FactoryTalk
user accounts or Windows Account security.
To set up automatic logout, specify the auto logout settings on the
Runtime
tab or the
Inactivity
tab of the
Project Settings
dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal