Example: Starting an application on a PanelView Plus CE terminal using parameters
You can use one or more parameters to start an application on a
PanelView Plus CE
terminal. For example, to start FactoryTalk View ME Station
and open an application called Malthouse
using all the parameters, from Windows Start
menu, select Run
and in the Open
box, type the following and press Enter
:"\Storage Card\Rockwell Software\RSViewME\MERuntime.exe" "\Storage Card\Rockwell Software\RSViewME\Runtime\malthouse.mer" /r /d /o /a
Alternative locations might be on
Storage Card2
instead of Storage Card
.Provide Feedback