Example: Starting an application on a MobileView terminal or a personal computer using parameters
You can use one or more parameters to start an application on a
MobileView
terminal or a personal computer. For example, to start FactoryTalk View ME Station
and open an application called Malthouse
using all the parameters, from Windows Start
menu, select Run
and in the Open
box, type the following and press Enter
:"C:\Program Files\Rockwell Software\RSView Enterprise\MERuntime.exe" "C:\ Users\Public\Public Documents\RSView Enterprise\ME\Runtime\malthouse.mer" /r /d /o /a
The example assumes that the .mer file is in the default folder.
Be sure to leave a space between the quotes in the middle or this will not work.
Provide Feedback