Set up an alarm

Use the Alarm Setup editor to set up an alarm.
To set up an alarm
  1. In the
    Explorer
    window, open the
    Alarms
    folder.
  2. Double-click the
    Alarm Setup
    icon to open the editor.
  3. Set up the options on the Triggers, Messages, and Advanced tabs.
  4. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal