Set up CSV export
Use the
CSV Export Setup
dialog box to set up CSV export.To set up CSV export
- From theExploretree, double-clickCSV Export Setupto open theCSV Export Setupeditor.
- Select theEnable CSV Exportcheck box.
- Select the types of information to be exported.
- Enter either or both of the paths to save the CSV files to.TIP:For example, enter:
- \My documentsor\Storage card2in.PanelView Plus 6orPanelView Plus 7pathIt is recommended to save CSV files to an external storage on aPanelView Plus 7orPanelView Plus 6terminal due to the limited space on the internal storage. Plug in the external storage to the terminal before running the application. If the external storage does not exist, theStorage Card 2orUSB Storagefolder will be created during CSV export on the internal storage.
C:\Users\Public\DocumentsinWindows PC or.MobileViewpath - Specify a tag or an expression for theExport Triggerconnection.
- (Optional) Specify a tag or an expression for theFile Labelconnection.
- (Optional) On theHistorytabs, specify tags forStatus CodeandStatus Message.
- ClickOK.TIP:Use theStartupeditor to turn on the CSV export function:
- Select theAudit trailcheck box to export audit information.
- Select theAlarmscheck box to export alarm information.
Provide Feedback