About CSV export

Use the
CSV Export Setup
editor to set up CSV export at design time to export audit, alarm, and diagnostics information to CSV files at runtime:
  • When the trigger's value changes from zero to nonzero.
  • If the trigger's initial value is nonzero when the application starts.
The CSV files will be saved to the specified path or paths. A CSV file name follows the format as YYYY_MM_DD_HH_mm_ss-<FileLabel>-TYPE.csv, where
TYPE
represents the type of information that could be
ALARM
,
AUDIT
, or
DIAGNOSTICS
. For example, an audit information CSV file name could be 2017_06_19_09_33_55-Batch001-AUDIT.csv.
TIP:
  • Storing more than 500 CSV files in a folder on an SD card may slow system performance.
  • Use CVB Data Log Tamper Detection Utility to detect the integrity of the CSV file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal