Reshape objects
To change the size of an object while maintaining its proportions
- Select the object.
- Grab a corner of the object.
- Hold downShiftand the left mouse button as you drag the handle.
- When the object is the desired size, release the left mouse button and then releaseShift.TIP:To grab a handle, point the mouse cursor at it, and when the cursor changes to a double-ended arrow, hold down the left mouse button.
To create a perfect square or circle
- Select the rectangle or ellipse object.
- Grab a handle then press and holdCtrl.
- Hold downCtrland the left mouse button as you drag the handle.
- When the object is the correct shape and size, release the mouse button and then releaseCtrl.
To reshape an arc or wedge
- Select the object, right-click to display the context menu, then selectEdit.
- Grab a handle and drag one way or the other until the arc or wedge is the desired shape.
- Click theSelecttool to end editing.TIP:The overall shape is the same size but the proportion that is an arc or wedge is changed.
To reshape a polygon or polyline
- Right-click the object and selectEdit.
- To create an angle along any line in the polygon or polyline, position the point on the line where you want the angle. A square is shown at this point.Drag the square to the tip of the angle.
- To delete a line segment, position the pointer at the tip of the angle, then click theDeletekey. The pointer becomes a cross hair when it is centered on an angle.
Provide Feedback