Context menu
The context menu opens when you click the right mouse button. The items shown on the menu depend on the object (if any) the mouse pointer is positioned over when the button is pressed.
TIP:
To select a command from the menu, click it or highlight it and press
Enter
.To close the menu, click anywhere outside it.
Provide Feedback