UseVariableMinMax

Choose whether the object's Minimum/Maximum values will use tag or expression values (True), or constant values (False), at runtime. If constant values are used, the MaximumValue and MinimumValue properties must be specified. If tag or expression values are used, the Minimum and Maximum connections must be assigned.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal