MaximumValue
Specifies the maximum value that the object can write to the Value connection. If the DecimalPoint property is Fixed position, the maximum applies to the stripped value, not the shown value.
If you assign a connection to the Optional Expression, the maximum also applies to the value sent to the expression.
If a Maximum connection is assigned, this property is disabled.
Provide Feedback