DecimalPoint

Specifies the type of decimal point to use:
  • Implicit
    if the operator manually enters the decimal point and you want the decimal point to be used when the value is sent to the Value connection.
  • Fixed position
    if the values to enter in the numeric pop-up scratchpad or keypad always have the same number of digits after the decimal point. If you select this type of decimal point, specify a value for the DigitsAfterDecimalPoint property. The decimal point is stripped when the value is sent to the Value connection.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal