MinimumValue
Specifies the minimum value that the object can write to the Value connection. If the DecimalPoint property is Fixed position, the minimum applies to the stripped value, not the displayed value.
If you assign a connection to the Optional Expression, the minimum also applies to the value sent to the expression.
If a Minimum connection is assigned, this property is disabled.
Provide Feedback