Create a linear gauge
The linear gauge displays a control's value from the data source on a linear scale. The
value indicator moves along the gauge to reflect changes in the value, allowing
operators to quickly assess the status and performance of the system. You can configure
thresholds to alert operators of specific states or alarm conditions. These alerts help
with proactive monitoring and maintenance to prevent errors or failures.
To create a linear gauge
- In FactoryTalk View Studio, in theGraphicseditor, selectObjects>Gauge and Graph>Linear Gauge. You can also click the linear gauge icon in the toolbox.
- Drag the mouse to position and draw a rectangle the general size and location you intend the linear gauge to be.
- In theLinear Gauge Propertiesdialog box, on the tabs, configure the linear gauge appearance, target value, setpoint, thresholds, control limits, its tags, and sparkline.
Provide Feedback