CSVDataLog ActiveX control

The CSVDataLog ActiveX control is similar to the DataStorePlus ActiveX control and contains the following enhancements:
  • Supports a minimum periodic logging rate of 250ms
  • Generates the CSV data log files which contain tamper detection strings
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal