Configure how the data being collected is stored in a log file
You may need configure how the data being collected is stored in a log file.
To configure how the data being collected is stored in a log file:
- Double-click the CSVDataLog or the DataStorePlus ActiveX control to open itsPropertiesdialog box.
- On theAdvancedtab, specify each options.
- ClickOK.
Provide Feedback