DataStorePlus ActiveX control
The DataStorePlus ActiveX control is similar to the RSView32 and SE data log model and contains the following advanced features:
- Specify when new files are created and old files are deleted
- Customize the headers of the CSV or TXT files
- Log periodically based on the time interval specified
- Each record is automatically date and time stamped with UTC or System Date and Time information
- Overwrite oldest data when the file reaches the size specified
- Log assigned connections only
Provide Feedback