Options on the General tab of the ME Chart Control Properties dialog box
The following table shows the options on the
General
tab of the ME Chart Control Properties
dialog box.Options | Descriptions |
|---|---|
Chart title | Specify the chart title that shows at runtime. |
Display Chart title | Select this check box to show the chart title at runtime. Click the Font button to specify the font. |
Title value options | Specify the chart title.
|
Redraw mode | Specify how often the chart updates with new data. |
Controlled by tag | Select this option to update the chart as the Redraw connection tag value changes. |
Automatic | Select this option and enter the redraw rate to update the chart at regular time intervals. The Redraw Rate controls how often to refresh the chart in millisecond, second, minute, or hour. The redraw rate is from 50 milliseconds through 596 hours. |
Maximum tag update rate | Specify the maximum rate at which the tags of the chart are updated. The default maximum rate is one second. |
Chart display options | Specify how the chart shows at runtime. |
Background color | Specify the background color for the chart. Click the color square and select a color from the palette. |
Use Gradient Style | Select this check box to show a gradient background. |
Data point connection | Select an option to specify how data points on the chart are connected.
|
Chart radix | Select an option to specify the number base (including decimal, hexadecimal, or octal) that is used to show numeric values on the chart. |
Chart orientation | Select the fixed axis to define the orientation of the chart.
|
Provide Feedback