Chart UDT members
The following table shows the Chart UDT members.
Members | Descriptions |
|---|---|
Title | This is the caption shown on top of the chart. |
NumberOfDataPoints | The is the number of data points in each DataSeries[] array. |
X_Axis_Label | This is the caption shown below the x-axis. |
X_Axis_Min | This specifies the minimum value of the x-axis. |
X_Axis_Max | This specifies the maximum value of the x-axis. |
Y_Axis_Label | This is the caption shown beside the y-axis. |
Y_Axis_Min | This specifies the minimum value of the y-axis. |
Y_Axis_Max | This specifies the maximum value of the y-axis. |
DataSeries_FixedAxis | This is an instance of the UDT DataSeries. This contains the data points of the fixed axis. You can configure the axis in the Chart orientation area on the General tab of the ME Chart Control Properties dialog box. |
DataSeries_x | This is an instance of the UDT DataSeries. This contains the data points for one data series of x-axis or y-axis, depending on the chart orientation. x is a number from 1 through 8, such as DataSeries_1, DataSeries_2, and DataSeries_8. |
Provide Feedback