Multiple version support

You can use the current release of
FactoryTalk View Studio
to create ME runtime application files (*.mer) that will run on previous versions of ME Station. These choices are available in the
Create Runtime Application
dialog box.
Open applications
Opening an application that was created with an earlier version of
FactoryTalk View Studio
or RSView Studio will convert the application to the current version of
FactoryTalk View Studio
. Once the application has been converted, it cannot be opened by earlier versions of
FactoryTalk View Studio
or RSView Studio. However, you still have the option of creating runtime application files that will run on earlier versions of ME Station.
Import applications
When you import earlier version application files,
FactoryTalk View
creates a copy of the application for the current version of
FactoryTalk View
. The earlier version is not altered.
You cannot import applications to
FactoryTalk View Studio
that were created with later versions than the one they are presently running.
TIP:
When a runtime file for an earlier version is created, the test run behavior on the current version of
FactoryTalk View Studio
may not be the same as actual runtime behavior on the targeted release.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal