Configure startup settings
Use the
Startup
editor to specify which project components to start at runtime.To configure startup settings
- In theSystemfolder in theExplorerwindow, double-click theStartupicon.
- Select the project components to use when the project starts.x
- Specify the data log model to use, if any.
- Specify startup and shutdown macros, if any.
- Specify up to five graphic displays to open at startup, along with a parameter file or list, if any. If there are no graphic displays, or if no display is selected in the list, an empty window is shown at startup.
- ClickOKto confirm the configuration and exit from theStartupeditor.
Provide Feedback