Set up global Memory connections
Use the
Memory
tab of the Global Connections
editor to set up global Memory connections.To set up global Memory connections
- On theMemorytab, in theMaximum update rate (seconds)box, select the maximum rate at which the data source will supply data to the global connections.
- Assign tags to the following connections:
- Assign a tag or an expression to this connection:
TIP:
To unassign a control, select the control in the
Tag
or Expression
column and do one of the following:- PressBackspaceon your keyboard repeatedly to remove the assignment one character at a time.
- Double-click twice to highlight the text, and then pressDeleteorBackspaceto remove the entire assignment at once.
Provide Feedback