Total RAM Usage

When this connection is assigned, and the Remote RAM Usage connection is set to a non-zero value, the application writes the total kilobytes of RAM being used by all the processes running on the terminal, to this connection, once every 10 seconds.
A read-write connection. Assign an analog tag.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal