ME Runtime RAM Usage
When this connection is assigned, and the Remote RAM Usage connection is set to a non-zero value, the application writes the kilobytes of RAM being used by the runtime application to this connection, once every 10 seconds.
A read-write connection. Assign an analog tag.
Provide Feedback