Set up global Display connections
Use the
Displays
tab of the Global Connections
editor to set up global Display connections.To set up global Display connections
- On theDisplaytab, in theMaximum update rate (seconds)box, select the maximum rate at which the data source will supply data to the global connections.
- Assign tags or expressions to the following connections:
TIP:
To unassign a control, select the control in the
Tag
or Expression
column and do one of the following:- PressBackspaceon your keyboard repeatedly to remove the assignment one character at a time.
- Double-click twice to highlight the text, and then pressDeleteorBackspaceto remove the entire assignment at once.If you have selected theUse Parameter Listconnection on theDisplaytab of theGlobal Connectionseditor, be sure to fill in theParameter Tagconnections n numeric order. For example, do not assign Parameter Tag #1 and Parameter Tag #3 without assigning Parameter Tag #2.Do not assign an expression consisting of a constant to the Remote Display Number. If you do, the display whose number matches the constant opens and can never be closed or changed.If a remote display print is in progress, the application ignores subsequent print requests from the data source until the display print has been processed.
Provide Feedback