Remote Display Print

Assign an analog or digital tag or an expression to this control to allow the data source to trigger the printing of graphic displays. The application reads the value of the control and prints the currently visible display when the value changes from zero to a non-zero value. Everything on the screen is printed, including the current display, pop-up windows, and any visible background applications.
Turn off the screen saver if you assign this control.
While a display is being printed, subsequent print requests from the data source are ignored until the display print is finished.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal