Close All On Top Displays
When this connection value is
True
, the application will close all replaceable On Top
displays whose display number is not 0. Non-replaceable On Top
displays will not be closed.If you want to use global connections, you must make sure that each display has its own unique number.
A read only connection. Assign a digital tag or an expression to this connection.
Provide Feedback