Name the application
Use this dialog box to name the application.
- For the rename operation, if the name is the same as an existing application, an error message will show. If the name is valid, the operation will proceed.
To name the application
- In the text box, type a name for the application, and then clickNextorFinish.
When you enter a new application name, do not exceed 32 characters. If the application name exceeds the maximum 32 characters allowed by
FactoryTalk View Studio
, errors and warning messages will show.Provide Feedback