Copy an application
Use this dialog box to copy an application.
TIP:
When you copy an existing application, the entire contents of the application, including the HMI server and all referenced data servers, will be copied.
To select an earlier version of application to copy, convert the application to current version in
FactoryTalk View Studio
before the operation.To copy an application
- SelectCopy applicationand clickNext.
- From the list, select the application to copy, and then clickNext.
- Type the name of the new application and clickFinish.
If the name is the same as an existing application, you will be prompted to overwrite the existing application. If you want to overwrite it, click
Yes
. If you do not want to overwrite it, click No
and enter another name.
TIP:
When you enter a new application name, do not exceed 32 characters. If the application name exceeds the maximum 32 characters allowed by
FactoryTalk View Studio
, errors and warning messages will show.Provide Feedback