Restore an application
Use this dialog box to create an application from an application archive (*.apa) file.
When restoring an application, you will not be prompted to validate user rights, and the security configuration of each project is preserved.
To restore an application
- SelectRestore applicationand clickNext, or double-click the *.apa file to launchFactoryTalk ViewME Application Manager.
- Select the archive file that you wish to restore. You can click theBrowsebutton (...) to search for and select the file. The default location for backup archives is\Users\Public\Public Documents\RSView Enterprise\ME\Archives
- ClickNext. If the archived application is passphrase protected, enter the correct passphrase and clickOK.
- Enter the name of the new application to be created from the backup archive. The default name will be the name of the application that was originally archived.TIP:When restoring an application, if the name is the same as an existing application, you will be prompted to overwrite the existing application. If you want to overwrite it, clickYes. If you do not want to overwrite it, clickNoand enter another name.When you enter a new application name, do not exceed 32 characters. If the application name exceeds the maximum 32 characters allowed byFactoryTalk View Studio, errors and warning messages will show.
- ClickFinish.
The restore process begins. If the name is valid, a progress bar appears.
Provide Feedback