FactoryTalk View Application Manager

How do I open the Application Manager?
Use one of the following methods:
  • From Windows
    Start
    menu, select
    All apps > Rockwell Software >
    FactoryTalk View
    ME Application Manager
    .
  • In
    FactoryTalk View Studio
    , from the
    Tools
    menu, select
    Application Manager
    .
Use
FactoryTalk View
ME Application Manager to perform operations on
FactoryTalk View ME
applications.
Use this tool to:
  • Copy an application
  • Delete an application
  • Back up an application
  • Rename an application
  • Restore a previously backed up project or application
    TIP:
    You must use the
    FactoryTalk View
    ME Application Manager for these operations. Attempting to use some other means may produce undesirable results.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal