Select an application
The list contains all the applications eligible for the operation.
To select an application
- From the list, select the application on which to perform the specified operation, and then clickNext.
Provide Feedback