Audit messages from a MobileView, PanelView Plus 7, PanelView Plus 6, PanelView Plus, PanelView Plus Compact, or PanelView Plus CE terminal
A
MobileView
, PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, PanelView Plus Compact
, or PanelView Plus CE
terminal cannot directly collect audit messages for FactoryTalk AssetCentre
. To receive audit messages, you need configure the FactoryTalk
computer and the MobileView
, PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, PanelView Plus Compact
, or PanelView Plus CE
respectively to collect the audit messages, and forward them to the FactoryTalk AssetCentre
server.Provide Feedback