Configure the MobileView, PanelView Plus 7, PanelView Plus 6, PanelView Plus, PanelView Plus Compact, or PanelView Plus CE terminal for remote audits

To collect audit messages from a
MobileView
,
PanelView Plus 7
,
PanelView Plus 6
,
PanelView Plus
,
PanelView Plus Compact
, or
PanelView Plus CE
terminal on the
FactoryTalk
computer, you need configure the terminal for remote audits.
To configure the
MobileView
,
PanelView Plus 7
,
PanelView Plus 6
,
PanelView Plus
,
PanelView Plus Compact
, or
PanelView Plus CE
terminal for remote audits
  1. On the terminal, start
    FactoryTalk View ME Station
    .
  2. Select
    Terminal Settings > Diagnostics Setup > Remote Log
    and click
    Edit
    .
  3. In the
    Address
    text box, enter the IP address of the
    FactoryTalk
    computer.
  4. In the
    Port
    text box, enter the port number from the
    FactoryTalk
    computer and click
    OK
    .
  5. In the
    Diagnostics Setup
    dialog box, select
    Message Routing
    and click
    Edit
    .
  6. Select
    Remote Log
    and press
    Enter
    .
  7. To ensure the capturing of all available information, select all the check boxes in the
    Remote Log Message Routing
    dialog box and click
    OK
    .
For the changes to take effect, restart the terminal.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal