Configure the FactoryTalk computer for remote audits

You need configure the
FactoryTalk
computer to collect the audit messages from a
MobileView
,
PanelView Plus 7
,
PanelView Plus 6
,
PanelView Plus
,
PanelView Plus Compact
, or
PanelView Plus CE
terminal.
To configure the
FactoryTalk
computer for remote audits
  1. On the computer that will be collecting the remote audits, start
    FactoryTalk Administration Console
    and log in to the Network directory.
  2. From the
    Tools
    menu, select
    FactoryTalk Diagnostics
    > Setup
    .
  3. From the root of
    Diagnostics Setup
    , select the check box for
    Enable this computer to receive messages broadcast from Windows CE devices or
    MobileView
    .
    The default
    Port
    number is 4445. You need configure the port number on the terminal.
  4. From the Diagnostics Setup tree, select
    Message Routing
    . Select the check box for
    Accept message from Windows CE devices or
    MobileView
    .
    If
    FactoryTalk AssetCentre
    is installed on the computer, the
    Secured
    check boxes are selected in each column by default. To ensure all audit and event messages are received, select all the check boxes for
    Error
    ,
    Warning
    ,
    Info
    , and
    Audit
    in each row, including
    Operator
    ,
    Engineer
    ,
    Developer
    , and
    Secure
    .
  5. Click
    OK
    .
Make a note of the computer’s IP address, which will be used in configuring the terminal.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal