Options on the Download tab
The following table shows the options on the
Download
tab.Options | Descriptions |
|---|---|
Source file | Type the path to the source file or click the Browse button (…) to open the Select File dialog box, browse for the source file, and click Open .If you want to select a font file, in the Select File to Download dialog box, select True Type Font Files (*.ttf, *.ttc) . |
Download as |
|
Destination storage type | Options include:
|
Run application at start-up | If you want the transferred runtime application to start as soon as the download is finished, select this check box. |
Replace communications | If you want the FactoryTalk Linx communications file in the downloaded application to replace the FactoryTalk Linx communication file presently on the terminal when the application starts, select this check box.This check box is only available when the Run application at start-up check box is selected. |
Delete Log Files | If you want to delete the log files when the application starts, select this check box. This check box is only available when the Run application at start-up check box is selected. |
Select destination terminal | The FactoryTalk Linx communication tree shows all the hardware available on the network. |
Provide Feedback