Font files
Licensed fonts for
PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, PanelView Plus Compact
, and PanelView Plus CE
terminals are supplied on the Accessories or Fonts CD. You can use only the fonts provided on these CDs with your terminals.Before downloading the fonts to a
PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, PanelView Plus Compact
, or PanelView Plus CE
terminal using ME Transfer Utility, copy the desired font files to the following folder on the development computer (source):\Users\Public\Public Documents\RSView Enterprise\ME\Runtime
This folder is created when
FactoryTalk View Studio
or FactoryTalk View ME Station
is installed.Provide Feedback