Compare a local file to a remote file
Use the
Compare
tab of the Transfer Utility
dialog box to compare a local file to a remote file. The local file is a valid FactoryTalk View ME Station
runtime file (.mer) located on the computer that is running ME Transfer Utility, or on a computer connected to that computer by a network. The remote file is a valid FactoryTalk View ME Station
runtime file (.mer) located on a remote MobileView
, PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, PanelView Plus Compact
, or PanelView Plus CE
terminal connected to the local computer by a network.To compare a remote file to a local file
- On theComparetab of theTransfer Utilitydialog box, from theFactoryTalk Linxcommunications tree in theSelect remote terminalarea, select the remote terminal whose runtime application file you want to compare to the local file.
- From theRemote storage typelist, select the kind of storage the file is stored in on the terminal.
- In theRemote filebox, specify the remote file to be compared. Click theBrowsebutton to browse for the file.
- In theLocal reference filebox, specify the local file to be compared. Click theBrowsebutton to browse for the file.
- ClickCompare.
The remote file is uploaded and saved to a temporary location on the computer running ME Transfer Utility. Once the upload is completed, the uploaded file is compared to the specified local file using a simple binary comparison. The utility then reports that the files are identical or different. When the comparison is finished, the uploaded file is deleted automatically.
Provide Feedback