FactoryTalk View graphic XML file
The
FactoryTalk View
graphic display XML (Extensible Markup Language) file is an XML document that describes an entire graphic display, including:- Display settings
- Graphic objects
- Properties
- Connections
- Animations
- Key assignments
- Grouping
- Wallpaper
A
FactoryTalk View
graphic display XML file contains the following parts:- XML declaration
- XML element
- Root element
A
FactoryTalk View
graphic display XML file may contain the following elements, attributes, and characters:- XML elements and attributes
- displaySettings element
- Graphic object elements
- group elements
- Special characters
The easiest way to understand how the parts of a display relate to an XML file is to create a display, add objects to it, and export the file and see how it describes the display.
TIP:
- Use theGraphics Import Export Wizardto import and export the XML information about graphic displays, and modify the exported files using a text editor such as Notepad.
- Picture or OLE object does not support XML import or export.
To determine whether an XML file is well-formed, open the file in Internet Explorer. If the XML code appears in Internet Explorer, the file is well-formed. If the file is not well-formed, Internet Explorer will show an error message. Advanced users of XML can create XML documents programmatically using programs such as Microsoft Visual Basic and Microsoft Visual C++. For more information about XML, go to https://www.w3.org/XML/.
Provide Feedback