XML element

In an XML document, the start and end of an element shows as follows:
<element name> ... </element name>
If an element has no sub-elements, it can end with
/>
, such as
<element name...attributes.../>
. For example,
<text name="Text1" height="16" width="87" left="69" top="42" caption="Pump House 1"/>
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal