Example: Graphic display XML file

The following XML file example shows a
FactoryTalk View ME
graphic display with a few objects on it, including a text object, a numeric display object, a numeric input enable object and a group containing two rectangles, one of which is animated. Not all the possible properties for these objects are shown in this file. Any objects or properties that are not listed will not be modified when the file is imported.
You can specify multiple attributes for an element, and have multiple elements.
<?xml version="1.0" encoding="UTF-8"?> <gfx xmlns:xsi="http://www.w3.org/2001/XMLSchema-instance" xsi:noNamespaceSchemaLocation="Gfx-ME1.xsd"> <displaySettings displayType="replace" backColor="white" width="640" height="480"/> <text name="Text1" height="16" width="87" left="69" top="42" caption="Pump House 1"/> <numericDisplay name="NumericDisplay1" height="44" width="104" left="234" top="150" borderStyle="raisedInset"> <connections> <connection name="Value" expression="{[clx1]Count_Up[0]}"/> </connections> </numericDisplay> <group name="Group1" wallpaper="false"> <rectangle name="Polygon1" height="35" width="53" left="378" top="40" visible="true"/> <rectangle name="Polygon2" height="35" width="56" left="428" top="85 visible="true"/> <animations> <animateVisibility expression="system\BlinkFast" expressionTrueState="visible"/> </animations> </group> <numericInputEnable name="NumericInputEnable1" height="55" width="80" left="57" top="142" keyAssignment="F1"> <caption fontFamily="Arial" caption="Stop"/> <connections> <connection name="Value" expression="{[clx1]n7[0]}"/> </connections> </numericInputEnable> </gfx>
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal