Create a new component
Some editors, such as the
Graphics Display
, Macros
, and Parameters
editors, can create multiple components (or files). If an editor can create multiple components, its context menu includes New
and Add Component into Project
. Editors that cannot create more than one component only have Open
on their context menus.To create a new component, use one of the following methods:
- Drag the component icon into the workspace.
- Right-click the editor and selectNew.
- From theFilemenu, selectNew, and then select the type of component to create.
TIP:
To copy an existing component
- In the Explorer window, select the editor that will use the component.
- Right-click the editor and selectAdd Component into Project.
- In theBrowserwindow, navigate to the location of the component you want to copy.
- Select the component and clickOpen.
Provide Feedback