The Explorer window

The
Explorer
window is the main tool for working with
FactoryTalk View Studio
. It lists the editors you use to develop your application, as well as the components, such as graphic displays.
The
Explorer
window has two tabs:
  • The
    Application
    tab contains the editors for creating and editing your application, and the
    System
    folder for setting up
    FactoryTalk
    Security.
  • The
    Communications
    tab contains the communications tree for the development computer. For more information about using the communications tree, see Help for
    FactoryTalk Linx
    .
Use the
Explorer
window to:
  • Open
    FactoryTalk View Studio
    editors
  • Open components
  • Set up
    FactoryTalk Security
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal