Draw an ellipse
Use the
Ellipse
tool to draw and oval or circle.- InProject view, double-click the container to include the object.
- In the editor toolbar, selectEllipse.
- In the editor, position the crosshair where the ellipse is to begin.
- Drag the ellipse to the end position.The object appears in the editor and inProject view.
- (optional) InProperties, edit theAppearancesettings:
- Visible. Show the object at runtime.
- Enabled. Enable interaction with the object at runtime.
- Opacity. Opacity level of the object in percentages. Set to0to make the object transparent.
- Blink. Blink the object at runtime.
- Rotation. Rotate the object around its center point (in arc degrees). Positive values rotate the object clockwise; Negative values rotate the object counterclockwise.
- Border color. Color of the border of the object.
- Fill color. Fill color of the object.
- Border thickness. Thickness of the object border in pixels.
- Hit test visible. Intercept user selections. False by default - user selections are not intercepted and are passed to the underlying object.
- Move target. See Make a graphic object movable.
- (optional) To resize, move, or align the object, see Graphic objects layout.
To group drawing objects, see Group drawing objects.
oval
circle
drawing tool
Provide Feedback