Group drawing objects

Group drawing objects so that they move together.
  1. In the editor, draw an object such as a rectangle or an ellipse and then draw another object within the first object.
  2. In
    Project view
    , drag an object under another object. The object that you drag appears within the object under which you drag it.
    TIP: You can move a drawing object off another drawing object and the objects still move together. Resizing one drawing object in a group does not resize any other drawing object in the group.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal