Objects
    An object is an element that represents a physical or non-physical component in the project. A type is a model or template object for creating instances of an object.
Create objects from 
Project view
 or Type view
. Change the properties of an object to change the appearance and data values displayed for that object at runtime.Provide Feedback